This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3806 Ct Terminal in case SHUTDOWN=High

Other Parts Discussed in Thread: UCC3806

 

Hello

Please let me know the status of  'Ct'  terminal  in case UCC3806  SHUTDOWN pin #16 is High .

We see  the description in the UCC3806 data sheet page6 (TERMINAL FUNCTINS) that

A_out & B_out  forced low  when SHUTDOWN is asserted.

Here is the question

Q1

If CURLIM (#1 ) .were below 350mV, then shutdown is NOT  latched...

So, I guess  Ct (clock  circuit ) does NOT stop even though SHUTDOWN is high...

My understanding above  is correct?

Q2

If CURLIM (#1) were above 350mV, then shutdown is latched...

In this case , Ct ( Clock cicuit : data sheet p8 ; atteched )  Stops ??

(  there are no signal path from  SHUTDOWN  to clock circuit directly....

My understainding is correct?)

Q3 

 My customer is using  two UCC38067s with synchronizing .

If SHUTDOWN is asserted in the Master, then Slave is also stop the output because Ct is stop?

 

Please let me adivise within 2days? 

Best Regards