I have been asked to provide a power supply with the following specifications:
- Non-Isolated
- AC/DC input
- The AC input terminals already have a bridge rectifier input on the ac side is 12 to 30Vac
- Input range for the DC terminals is 12 to 50Vdc
- Input current is limited to 100mA via a polyfuse
- Output 1: 3.3Vdc @ 250mA
- Output 2: 5.0Vdc @ 50mA
So there are many possibilities.......
- Use a simple switcher for example a LM2594HV for the 5.0V output and then use a LDO linear regulator to step down to 3.3V
- +Simple
- - Not very efficient
- Use two simple switchers for example a LM2594HV for the 5.0V output and another for the 3.3V output
- +Simple enough
- +Efficient
- - Not sure if having two of these running in parallel will create EMC issues
- Use a dual output switcher possibly a LM34910C
I would to hear your thoughts and recommendations from the power supply guru's