We are using a power supply with output 40V x 3A and we have problems to adjust the current in 4 channels.
Using only one channel we can adjust the current (700mA) and it stay stable, but when we increase more channels the current goes down (380mA) and isnt stable.
we are using it to connect 12 leds with Vf 2,9V for each channel and the circuit is mounted as AN-2071