Gents,
I would like to design a wide Vin application using TPS54061-Q1 for an automotive application running from a 24V battery. Here are the design parameter.
Primary Regulator TPS54061-Q1:
- Vin-max = 60 V
- Vin-min = 8.5V
- Vout = 12 V
- Iout = 0.15A
- In case of Vin < Vout we expect to see that Vin roughly follows Vout and the regulator stays stable under this condition. This is important in case a cascaded LDO generates a 5V from Vout (12V) rail
- UVLO as low as possible
Can you please comment these requirement with focus on the Vin < Vout topic. We expect to see that Vin roughly follows Vout and the regulator stays stable under this condition down to 8.5V
I also appreciate your recommendation with regards to
- Highest Switching frequency and still meeting minimum on-time with an adequate margin since on time is shown as typical value
- resistor values at the Enable pin for wide Vin operation from 60V down to 8.5V
Thanks & Regards,
Alexander