Hello everyone,
as I am trying to use the Fusion Digital Power Designer for power measurements (Voltage and current). It is planned to use a UCD9240 or UCD9222 as management IC and two or four PTD08A006W power modules connected, as those are compatible with Fusion Digital Power Designer. In the latter case each power branch can be sourced by one of the four PTD08A006W (1V and three times 3.3V) modules. As four modules require much space on a PCB board, I thought about using only two PTD08A006W (1V and 3.3V) modules and put three LM25056 power measurement circuits for the remaining 3.3V power branches.
Now I would like to know whether it is possible to configure and use the LM25056 over PMBus in the Fusion Digital Power Designer for measurement purposes?
For the LM25056 an PMBManager application was available, but I wasn't able to find it. Is there a new Version that would allow power measurements?
Thanks in advance
best regards