I find LP3950 color LED driver, and there is example of the Typical Application:
I want to use it in color organ controller with 12V RGB LED light strip 5050. The LED light color changes need be synchronized to audio signal with both amplitude (beat) and frequency methods (4 channels). The audio input will be on-board electret microphone, and also 3.5mm audio input.
I know that I should use spectral decomposition of the signal by harmonics of the input signal. The input audio signal should be filtered into one of four categories by frequency: low, medium, medium-high, and high. Each frequency category is then assigned a specific pulse width modulated output that feeds to the color RGB SMD LED light strip. How to modify this schematic for my purpose?