Hello,
I hope someone can help with this. I'm using the LM46000 to produce a +3.8V output from an input range of +5V to +30V. If Vin starts fairly low (say 7-8V) the circuit sticks in PWM mode and its current consumption (even with load disconnected) never goes below 5-7mA. If, leaving everything else untouched, Vin is raised the circuit suddenly enters PFM mode (at a Vin value of around 12-15V in our case) and current consumption becomes acceptable (around 70 microamps). If Vin is now lowered back to a low value the circuit stays in PFM mode and current consumption is low ... exactly the behaviour mentioned near the top of page 16 of the datasheet.
We need to somehow avoid this behaviour. The circuit's output voltage has no trouble reaching the programmed +3.8V output so I don't understand the datasheet comment "... the LM46000 may not enter PFM mode if the output voltage cannot be charged up to provide the trigger to activate the PFM detector." What isn't being "charged up"?
FYI, the circuit values came from the WebBench online application; L=120uH, R(RT)=33k (so around 1MHz PWM frequency), CFF=10pF ....
Thanks a lot in advance - Paul.