Hi,
I am looking to build a 3 phase power supply based on T I devices. The specs are as given below :-
Input : 3 phase – 3 wire (R, Y, B) – 440V – line to line
Outputs : 5V / 7A, 24V / 3A and 24V / 2A – all 3 outputs isolated from each other
Kindly suggest suitable reference design
Regards
Atul Bhakay