Hi,
We are using the Device TPS2592BA for one of the SSD designs.
1) Is it mandatory to use the Back FET drive functionality (BFET: Pin 9)
2) Can the pin BFET (pin:9) be left as floating, If not using the BFET function?
Regards,
Akshat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using the Device TPS2592BA for one of the SSD designs.
1) Is it mandatory to use the Back FET drive functionality (BFET: Pin 9)
2) Can the pin BFET (pin:9) be left as floating, If not using the BFET function?
Regards,
Akshat
Hi Akshat,
This device falls under the Power Interface group. I will go ahead and move this post to their forum.
Regards,
Alek Kaknevicius
Hello Akshat,
No, it is not mandatory to use the BFET functionality, Though this is a special feature we have in this part. it prevent Holdup capacitance energy to dump back by blocking reverse current flow from output to input whenever input fails
Yes , you can left it floating if not used.
Who is the customer and potential of the opportunity?
Regards
Dinesh