This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24262 / Internal bias regulator voltage

Other Parts Discussed in Thread: BQ24262

Hi All,

Let me ask about Internal bias regulator of bq24262. I understand that internal bias regulator is powered from VIN and the output voltage can be seen on DRV pin. Then I have some question as below.

  • I think the variation of output voltage range is slightly large. Does it mean that it vary from 5.3V to 4.3V between part to part?
  • I'm not sure that the maximum rating of DRV pin is 5V though VDRV(max) is 5.3V. Please explain this relationship.

Best Regards,

Sonoki / Japan Disty