Hi
I just the LM5122EVM-1PH eval board and so far it is working flawlessy for my application. However, I need to change the operating voltage range. currently its 9-20 in, 24V out @4.5A, I need to run down to around 6V but max could be around 14-16
what is the simplest way to change the input range? (webbench wants to change almost every component sigh)
Thanks
Rich