This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51620 system hang on issue (urgent)...

Other Parts Discussed in Thread: TPS51620

Dears,

My customer use Intel Core 2 Duo P8400 (2.26G, ICCmax:38A) and design with TPS51620 Vcore IC.

They found if the CPU cx-state is ON, then the system will hang on while the system resume from c3 to c0.

If they turn off cx-state function, system will not hang on!

They had tried to add 4 additional Cap. in parallel with output side but still fail.

Attached is customer schematics.

Is there anyone can give me some idea for debug?

Very appreciate!

SCHEMATIC1 _ 39. IMVP CPU VCore.pdf