as per technical document TPS62750 has VIN different and VCC different. No problem with VIN range but i have only available source is VIN that is 5V D.C. Can i use it for VCC also?
tested results for TPS62750 for 2A and 3A output current are at 12V VIN and VCC=6.5V
so can i use this whole scenario at
VIN=5 D.C, VCC=5V D.C
VOUT1=4V IOUT1=1.5A
VOUT2=4V IOUT2=2.5A
???