This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM6420-8.4, how to use for 4 batteries (16.8V)?

We have used the LM3420-16.8 in an application for many years. That 16.8V set voltage version got obsoleted, only the 8.4V version is available. The data sheet still says one can use this device for 1,2,3 or 4 cells. How do I do that? My problem is that it is used in a UL listed device, so i don't want to change the overall circuit, if possible.

Thanks,

Chris