Single Lithium cell input: 2.5 to 4 Volts in
40mA @ 6V out
Intrinsically safe => three zeners on either end of the inductor.
7.5V zeners being used. Have also tried 8.2V Zeners, but the 7.5 is preferred.
Zeners on the input, no problem. Zeners installed on the output side of the inductor kills performance.
Is there a way to change the basic design to accommodate the addition of these zeners?