Is there any way to immediately set the chip to Standalone mode while in Host mode or do we have to wait for the 50s watchdog timer to expire?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any way to immediately set the chip to Standalone mode while in Host mode or do we have to wait for the 50s watchdog timer to expire?
Jeff,
Are there any registers we can read to confirm that the charger is in standalone mode?
If the registers are reset to default values (in Standalone mode), can I just assume that any read of a register that was changed from the default setting in Host mode back to default settings confirms that I am in Standalone mode? For example, let say I set register #4 charge current to 100mA in Host mode and after the watchdog timeout the charge current s/b set to default (external ISET) in Standalone mode. When my code reads this register I can say that I am in Standalone by the fact that the register was reset to its default. Is this correct?
Rudy