Hi,
My customer is using LM3489 under the following conditions
Vin=12V Vout=6.2V Iout=1A and the sw frequency become around 250kHz.
and they changed the FET to which had a lower Rdson and higher gate capacitance
(changed On-semi CPH3355 to ROHM RQ1E050RP )
As the result, the Sw frequency was reduced to around 150kHz.
Is there any possibility that the FET specs make such a big impact on Sw frequency?
and the pin layout of these 2 FETs are different, so they jumpered between LM3489 PGATE pin and RQ1E050 GATE pin.
Actually I'm more concerned about an impact from the jumper.
Any advice would be appreciated.
Thanks
Go