We are running an LMZ14202 to create 5.2 V from a 12V input. I am experiencing problems with the circuit when running at low loads (<300 mA or so).
The output voltage is correct but very unstable, lots of noise and variation due to small changes in output current. For example, just turning on an LED that draws 6 mA is causing a 10 mV dip in the output voltage. The bigger issue is that the switching noise on the output is much worse and the switching frequency changes dramatically with load. I can actually hear the parts buzzing, and hear the pitch changing as the LED's turn on and off. The output waveform has periods where the switching cycles are present and then they go away, almost like it is PWM controlled or something similar.
I tried hooking up a sizable load resistor and all of this went away. The output was stable and there was a continuous switching waveform observable.
I may be able to load it down enough to solve this problem by adding dummy loads, but I am wondering if changing R_ON and the switching frequency can impact this. We are currently at 100k for ROn which is 400kHz. I was thinking of trying a higher frequency 500-600 kHz. Will this help?
Also, I could not find anywhere in the datasheet where minimum load currents are mentioned - is there a recommendation for minimum loading for this part?
Thanks for you help.
-Chris