Hi There
I have simulate some solutions about the resonant 160 amps welding inverter, I need a constant voltage version fase shift or a quasi resonant UC386* version with a voltage controlled oscillator, I need that for mig welding, a constant current is not suitable.
I do see and find a lot of possibilities, I do not now what driver for the igbt,s is better, a drive schip like the IR2110 or a transformer, first is more easy and fast but with welding is this suitable, a lot of welders use a forward, I think a half bridge is for me enough, but a full bridge is not so much more expensive.
Do someone here as a LTspice model of the UC 3868 or before, like UC 3860 until 68 and a good working version of UC3875/ UC3979 is fase shift not prone of trouble with welding dutys, maybe a variable frequency quasi resonant is better, making one from a tl494 is possible but not a constant voltage because there is no vco.
Thanks for the help.
kees ijpelaar holland.