This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

questions about DCH010505S

Other Parts Discussed in Thread: DCH010505S

when I use the DCH010505S,I have encountered some problems that when the input voltage is 5V,the output voltage is 7.6~8V. But according to the chip manual, the output voltage should be 5V.Can you help me?Thank you.

  • DCH010505S and all DCH series are unregulated isolated power converters.

    With exactly 5Vin  and no load on the Vout bus, the output voltage can be as high as 8V or slightly higher  with 0 load.

    Typically  with 20mA load( 10% of 200mA maximum load) , the published Vout with exactly 5Vin is about 5.6V. The data sheet  has load regulation from 20mA to 200mA .

    Tom