Dear TI
I’m using the BQ27441EVM-G1A with the EV2300 and the Battery Management Studio 1.3.40.
I connected a Li-based battery, I was fine, I mean, measure the voltage is perfect.
But I cannot update some battery parameters, i.e. Design Capacity. Let me present all the followed steps.
- I click the command SET_CFGUPDATE.
- I rewrite the Design Capacity.
- I click Write_All.
- I click again the command SET_CFGUPDATE.
- I Disconnect the Battery.
After that, the Design Capacity parameter returns to their original value. How can I make those changes permanent?
Thank you in advance.