This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3405A question of the Rzi calculation

Guru 20090 points
Other Parts Discussed in Thread: LM3405A

Hello,

I have the question of LM3405A about RZI calculation.
Please see the attached file.


LM3405A_RZI.pdf

I simulated the LM3405A with some Vin value( Vin=9V, Vin=18V, Vin=9V~18V)
As a result the Rzi values as the following.

Vin=9V , Rzi=634ohm
Vin=18V, Rzi=2.05kohm
Vin=9V~18V, Rzi=2.05kohm

I could find the calculation of Rzi from the datasheet P.10 and figure 17.
I think that we should choose 634ohm for Vin=9V~18V.
The Rzi is used for charge current for zener and boost cap.
Thus, the Vin(min) is worst case of charge current.
Is my understanding correct?

Thus , if we use E24 resistor, should we use 620ohm of Rzi for Vin=9V~18V, Vout=3.4V, Iled=700mA application.

Best Regards,
Ryuji Asaka