This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3050 CUV fault from cell insertion

We have a 4S1P configuration.  When we are installing the cells, the chip gets latched in a CUV state and turns off the discharge FET.  These are all new cells charged to 4.2V.  One way to clear this fault is to provide a positive charge current.  Our problem is that the charge circuit we have only charges to 16.4V and to provide a positive charge current with the new cells, we need to provide at least 16.8V which we are not.  Is there a command that can be sent to the chip to reset the chip and remove the CUV state?  

Thank you