Hi, two questions please,
1) In the LM2595 datasheet, requirements of the input capacitor states "Use caution when using ceramic capacitors for input bypassing, because it may cause severe ringing at the VIN pin." but WEBENCH suggests the Murata 1206 GRM 4.7μF Ceramic Multilayer Capacitor, 50 V dc X7R Dielectric as an input capacitor. What should I look out for if I want to use this capacitor as WEBENCH suggests? Input voltage for my application is between 21-26V and output is 15V @ 1A max.
2) The datasheet specifies that an input capacitor must be rated at least 1.5x the input voltage. Will a filter capacitor after a full-wave bridge rectifier also need to be specified at 1.5x the input voltage if it feeds the LM2595 circuit? I'm planning on using a 4700uF 35V filter cap for 26V max input voltage.