Dear Sir,
I am going design a boost circuit with high amount output capacitor (560uF),
my specification:
vin=5v, vout =16v/300mA, cout 560uF, L=3.3uH
Rcomp calculated value=4977K, Ccomp=0.8nF
According to the datasheet the Rcomp & Ccomp shuld be RCOMP < 120 kΩ and CCOMP> 820 pF, in this case what amount of Rcomp should I choose? or is it possible to use type III compensation? could you please give me some suggestion? Thanks.