Hello, I'd like to use the pdip TL5001 buck converter with over current protection on load current. But how? Another design to create the constant current source for a lead acid charger with max Vout limit. Also a design to power a 3.5V motor at 8Amp from 30Vin using over current protection. Motor does not need to be connected to 0V and can have low side current sense resistor. Thank you.