Hello everyone!
I am currently developing some tests using BQ24030EVM and I have detected a strange situation when charging the battery.
I have removed R9 so as to enable the TS capability and I found in first place, when charging in Fast Charge Mode, there is no problem, STAT1 LED is ON and the current measured through a multimeter into the battery is OK.
The problem comes when the battery reaches 4,05V and BQ24030 is swapping from Fast Charge to Termination Charge. In this proccess both STATX LEDs are blinking alternatively for more than half an hour and of course, the current sunk by the battery is swapping from 50 mA (more or less) to 130 mA (more or less) and this is precisely what I want to avoid.
Is there any way to perform a clean step from Fast Charge Mode into Termination Mode?
I hope to hear from you soon!
Regards.