Hi,
UC3825A is the controller of our buck circuit and the driver IC is ISL6207.
In the application, the input voltage is 20v and the output is 8.4v. the maximum loading is 8A.
During the test, i find that when CT value is less than 220PF, the UC3825 power loss will increase and OUTA output will be abnormal.
There is a abnormal pulse followed the high level signal of OUTA, which causes much power loss in our application.
Increasing CT value to above 220PF can solve this problem.
could you plese help tell why?
Best wishes,
Jacky