Hello, this is my first time because I really need help.
I'm trying to build a voltage regulator for tattoo machines. I'm almost cloning a commercial power suply and the regulator uses the LM2696 or LM2576 circuit. (I don't know wich component they are using because the reference is removed with a sandpaper.
I have identified the circuit but when I tried to design the circuit choosing the value of the aditional components, I realized the commercial power suply is oversized. The specifications are: Vi=24v Vomax=20V Imax 3A, with those specs I calculated a Inductance about 22uH, but the commercial suply inductor is about 90uH.
Also the capacitors are oversized: 470uF in the commercial and less for the theoretical value but this is less important, in my opinion.
I would like to understand why 90uH (real measure is about 87uH and nearest commercial value is 92uH, Würth elektronik 7447013 , but I can't get it in RS neither mouser etc..). I'm trying the circuit with other inductances and I don't see significant differences between 30uH and 150uH, but just connecting the tattoo machine, I don't have a oscylloscope. I want to know if I can put a 50uH or 150uH inductance and the possibles issues.The ircuit is the page 9 (second circuit) and it doesn't have capacitor in the Feedback.
I just want to know if it is the same with 50uH or 100uH (not any value, just more than the theoretical calculated in the table)
This is the schema of the commercial power supply
Thank you very much.