In LM3464 datasheet page no.10 under subsection Operation Principles of DHC, it is written that
when all the output channels are in regulation and the forward voltage of any LED
string decreases due to temperature raise, the drain voltage of the corresponding channel (DRx) increases to
exceed the default 0.9V typical headroom voltage in order to maintain constant output current. As the drain
voltage increases, the voltage of CDHC increases and the current sink into the OutP pin decreases. This will
finally result in decrease of rail voltage (VRAIL) until the corresponding DRx voltage returns to minimum level
If voltage of CDHC increases, actually the current sink into the OutP pin is to be increased? pls give explanation for this