Hi,
I am trying to use two LMZ31704 to get a 5V power rail @7A from 12V input. I am asking if I could not use an external clock to synchronize the 2 devices and instead, only set resistor to the AGND on the RT/CLK pin of the Master and the Slave and connect the SYNC_OUT output of the master to the RT/CLK of the SLAVE ?
Best Regards,
K. Stoffels