Gentlemen:
I am currently trying to create a new pack for a customer using the bq20z655 gas gauge. Since this is my first attempt using the new chip. I created a dummy .senc file using a bq20z90-equipped battery of similar configuration. When I try to migrate that .senc file to the bqMtester, I cannot get a device and version for the bq20z655, and using the default bq20z90V150 entry yields a "Single site InitCacheFromSetup() failed for board ti1. Error code =65557". My documentation lists Error code 65557 as "Header bad or format bad".
Is there an update to the bqMtester firmware that would include the bq20z655? Am I making other errors in the preparation of this pack? I suppose I could wait until I have the first pack built up and follow the instructions for creating a Golden Image, but would I still have problems migrating it to the Multitester?