Hello,
I have a question about the balancing feature of the bq29312A.
More precisely I don't understand well how the balancing is performed. Are there internal FETs in parallel with each cell? Or external FET are needed?
The datasheet states that the maximum current for cell balancing is 10 mA (absolute maximum ratings table). Is this value the maximum current I can draw from the cells during the balancing process? Is it possible to increase this value?
In my project I need to balance two or four 150-200 Ah lithium cells. So I need greater current for cells balancing.
Thank you in advance
Danilo