Can I use an EV2400 and BQSTUDIO to communicate via HDQ with a bq27541 that is integrated in a battery pack?
If so, how?
If not, what do I need to do so?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use an EV2400 and BQSTUDIO to communicate via HDQ with a bq27541 that is integrated in a battery pack?
If so, how?
If not, what do I need to do so?
Hi Randy, welcome to the forums!
Yes, you can use the EV2400 and bqSTUDIO to interface with TI gauges that use the HDQ interface (I have done so plenty of times). Just connect the HDQ and ground pins from the battery pack to the EV2400. As long as the protection circuitry in the battery pack hasn't been tripped (perhaps from over-discharge), you should be able to communicate with the pack. That said, the HDQ interface is pretty slow (7 kilobits per second), so you may notice that the software takes a while to update the Registers and Data Memory panels.
On that note, what sort of battery pack are you trying to interface with?
Hi Randy,
The EV2400 has technically supported HDQ for quite a while, but the reason it's listed as being unsupported is because it's a bit unstable. The newest firmware has improved its performance, but it's still a little inconsistent in terms of connection reliability; the older EV2300 adapter has more stable HDQ support but has only unofficial driver support in 64-bit versions of Windows.
If you haven't grabbed the latest firmware update for the EV2400, you can download it here (SLUC578).
Regards,
Jason
Hi Jason,
I set up bqstudio on my PC, upgraded EV2400 to v0.18 firmware and connected EV2400 port #3 to HDQ and Batt- on my battery pack. bqstudio now communicates with the battery (bq27541-G1), but I don’t know how to use bqstudio and the help files are very terse.
Questions:
Randy