Hi,
I intend to use the TPS5420 to buck a 18-22V to 6V@1A
I checked both the datasheet and the EVM usersguide
Formula 7 and 8 in the datasheet are to determine the ESR-max value. Calculating back from the datasheet example I do not understand formula 7. What is FLC? Is that the LC corner frequency that should be kept between 3-30KHZ?
That frequency should also be squared in the formula right?
If I simply follow the EVM component values (my output is 6V, EVM is 5V) the 100uF output cap is a special case requiring 80mOhm ESR.
Is it also allowed to take another cap, for instance a 100uF Sanyo Oscon with 30mOhm ESR and add a 40 - 50mOhm external series resistor adding up to 80mOhm ESR max?