This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hirotaka,
Initial accuracy is a measure of how close the reference voltage is to the expected voltage. As time passes in an energized circuit, the change in the reference voltage is determined by the long term stability specification.
The REF2025 has an initial accurary maximum of +-0.05%, which translates to no more than 1.25mV difference from 2.5V initially. As time passes, the part is specified to have 60ppm of drift long term (1000 hours). So, after 1000 hours, the part will be within:
2.5V +- 0.05% +-60ppm, or between
(2.5V *(1-0.0005) * (1-0.00006)) and (2.5V *1.0005) * (1.00006), which calculates to between
2.4986V and 2.5014V, or within 1.4mV of 2.5V
The LM4132 has the same initial accuracy, with lower long term drift of 50ppm instead of 60ppm, and is within 1.375mV of a 2.5V reference after 1000 hours.
Hope this helps you.
Chris
Chris san,
Thank you for your reply and your cooperation!
We got it , however we would like to confirm one point.
The LM4132's datasheet shows Long-Term Stability 0-1000 hours 60ppm.
So, even if the time passes 1000hours, Long-Term Stability is the same as 60ppm, isn't it?
We do need your help.
Kind regards,
Hirotaka Matsumoto