This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Advanced bqMTester software generates error code 65538 when connected to BQ20Z80

Other Parts Discussed in Thread: BQ20Z80, BQMTESTER, BQEVSW, EV2400

Hello everybody,

I'm having difficulties with MultiStationTester.exe software version 1.06 together with a "bq20z80 v1.02"-device. 

The behavior is similar to the one in "Advanced bqMTester software generates error code 65538 when connected to BQ20Z45R1"-Thread.

I chose bq20z80 v1.02 in the MultiStationSetup-Tool but if I start MultiStationTester.exe it shows bq20z80 v1.01 in the header. If I klick "Start" I receive the error code 65538.In the bqEvaluationSoftware it shows v1.02 correctly, also in SingleStationTester it shows v1.02. This behaviour occurs on a system with Windows 7 64Bit. However, if I use the same MultiStationTester Version on a system with Windows XP 32 Bit, the tool shows v1.02 correctly and I receive no error 65538. 

Am I using a wrong tool version? I'd like to use the Windows 7 system for production, how could one fix the problem?

Sincerely,

Sebastian