Hi,
I have a design that uses the TPS54040, peak power output is about 350mA and the design currently is working well. I'm having trouble sourcing the TPS54040 parts, but can get the TPS54140. I see that the power rating for the TPS54140 is 1.5A, can this be used as a drop-in replacement in my application? I don't see any other specification changes that would lead me to believe that it won't just work fine.
Thanks!