This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563210 minimum input voltage

Other Parts Discussed in Thread: TPS62130A, TPS62133

Hi All,

I need a 12 to 5 volt converter @3A max, for which the TPS563210 is perfect, but I'd like it to keep delivering about 200mA from a 2 cell Li-Ion battery if the mains fails. The datasheet recommends Vin be > Vo/0.65, or >7.7volts. Does anyone know if the 2 cell supply will work? It's close, but does exceed the duty cycle max recommended. The low output current when on battery should help ... but?

Thanks, Brian