Hi,
I want to configure UCD9222 connected to UCD7242 mosfet driver. I am using I2C protocol low-level configuration. I have been suggested the many ways of configuring the device using Fusion GUI, ROM and DSPs but I am interested in low-level configuration using just I2C. Can anyone direct me to UCD9222 specific script in order to know if I am missing anything?
I have an unconfigured UCD9222 assembled on the board with nothing but I2C connection via FPGA. The only option to configure the board is to use I2C protocol. I have fully functional I2C Write protocol (one byte at a time) and partial read with reading one byte. Please suggest me a specific bit-stream or sample configuration script for the same.
Thanks,
Pawan Ghotikar