I followed a design on Webench to convert 24 Vdc to 3.3 Vdc.
Schematics is the same but changed the layout a little bit
I am having a serious problem on the highlighted part (24V in), my modules are fried up, I often see a flame. I tested 20 modules, 10 of them are burnt with a flame.
Here are some examples of the modules. Either the highlighted line burns or the IC explodes.
I check by a DMM that there is no short circuit between Vin-Vout-GNDs. I inspected the connections with a microscope that looked fine.
Here is how I test the DC-DC converters. I supply 24V from a PSU, and place 1.8 M ohm resistor between Vout and ground to measure the voltage by an oscilloscope. (I know red should be used for V, not for Ground, it was just closest wire to me)
I suspected flux to reduce the resistance between the Vin - Ground, so I cleaned the boards, but the problem remains.
It seems like the board drawns too much current somehow, does anyone have a guess/idea what could be the problem?