Hi,
Are there any evaluation modules available for purchase with UCD9222 + UCD7242? Please suggest.
Thanks,
Pawan Ghotikar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are there any evaluation modules available for purchase with UCD9222 + UCD7242? Please suggest.
Thanks,
Pawan Ghotikar
There is a reference design PMP6730. We can share the design but there is no board for purchase.
There is a TMDSEVM6657 EVM that has UCD9222 and UCD7242. But it includes DSP and FPGA on the board.
If your purpose is to learn/test PMBus operation, you can purchase a UCD9224 EVM.
Regards,
Zhiyuan
Yes. TMDSEVM6657 has UCD9222 on the board. But it is a bit expensive because it also has FPGA and DSP on the board.
You will be able to test most commands using UCD9224 EVM, which is cheaper. But some commands are specific for UCD9222 (VID related, see PMBus reference document).
Good morning Zhiyuan Hu,
I am planning to get one ucd9224evm-464. Is this board supplied with USB to GPIO to connect with the computer and work on it using FUSION ?
Thanks,
Pawan Ghotikar