Hi There,
I am looking at using the LP38693-ADJ - 500mA Low Dropout CMOS Linear Regulators with Adjustable Output Stable with Enable pin. The datasheet states the quiescent current during shutdown (EN < 0.4) is 0.001uA typ / 1uA max.
Can you tell me the conditions for typ vs. max? e.g. If I operated between -20c and 60c what would be the Iq shutdown, running from a battery - say 4.2V to 3V.
My configuration is to output 1V8, using 6k2 and 12k.
Worst case, I'll put a FET in front to make the shutdown 100nA.
Many thanks,
James