This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51025 AD - AD/EN doesn't work properly

Other Parts Discussed in Thread: BQ51025

I'm currently using an ECH8654 PMOS switch for AD to VOUT connexion while using a DC plug.  But i've got a strange behaviour :

If I put a DC plug of more that 12V (i.e. 12.3V or 13V), it looks like AD/EN doesn't work properly and is just following AD voltage so that switch never goes on and AD plug looks disconnected.

When I'm using <12V DC plug, everythings looks fine.

Is there any good reason for that behavious ?

Note : I'm using a 2S schematic such the one that is present onto datasheet.

Thanks for help