I used Webench to create a 24 VDC upconverter from 12VDC. Over a couple weeks of running the upconverter stopped producing the 24VDC. I initially replaced LM3481MM, but it still didn't work. I then replaced the CSD17559Q5 Power Mosfet and the 24VDC upconverter started working. It is concerning that the MOSFET died and I would like it to be analyzed to give me an indication if the issue was contained within the package of the MOSFET or if it is a board layout issue.
Thanks,
Garrett Marshall