Hello,
I'm currently designing a board where I plan to use TPS62120. I have been examining the datasheet and I have some questions regarding it:
1) In table 7.5 current I_LIMF is defined only for V_in = 8V. I wonder how it changes depending on the input voltage? Are the values for 3.3V, 8V or 12V much different?
2) In equation (2) shouldn't there be [A] instead of [mA]?
3) I calculated C_ff according to equation (7) for R1=560k and obtained the value 11pF that is two times smaller than the one proposed in the table. I know it doesn't matter much, but is there a reason to go with 22uF?
4) In the Power Supply and Layout section there is nothing regarding bulk capacitor. Won't it hurt much if I will add a 100uF electrolytic capacitor before the input capacitor (main power source is couple of meters away)?
Excuse me for kind a pedantic questions, but I want to be very sure about each detail. Thanks in advance.