Hi TI experts,
I want to acquire higher current, so I use one UCD9244's channel to generate PWM signals to control two UCD74120 simultaneously.
Two FLT signals are connected to one OR gate and then the output of this OR gate is connected to the FLT pin of this UCD9244's channel.
But how to connect two Isenes signals to one CSA pin of one UCD9244's channel?
My schematics is like this
When I use the UCD9222 to connect two UCD7242s, UCD7242's Isenes is current related, so I can combine these two UCD7242's Isenes signals together.
Showing like this in the UCD9244's datasheet,
But now, the UCD74120's Isenes signals are voltage related.
1. Do I need one voltage adder? Could you show me some examples with least BOM?
2. Can I just leave the UCD74120's Isenes signals unconnected to simplify the schematics design? If the Isenes signals are unconnected that is the UCD9244 does not monitor the UCD74120's output current, can the UCD74120 work well to generate the right voltage output and reach the right output current?
Regards,
Feng