Hi Team,
Could you help answer the questions below I have from my customer please?
"My query is regarding the maximum input voltage... The absolute maximum voltage is specified in your datasheet as 76V. The maximum input voltage we can expect to experience is 66V which is easily in range. However here at Thales we have our own derating policy which means our own maximum allowable input voltage is 60.8V so we are in violation of our policy.
I am assuming you have your own safety margins which you abide by when specifying the absolute maximum ratings for device parameters.
Could you provide details of these safety margins?
Could you also inform me of what voltage the device has been tested up to and still worked?
Could you also specify what it is about the device which fails. Is it a complete electrical breakdown or is it thermal related?
Is the damage instantaneous at power up or will it fail after exposure for a duration?"
Many thanks in advance for your support on this.
Best regards,
Ross