Hi,
I am using PTH08000WAH for 12V to 3.3 V generation of following configurations.
Vin = 12V
Vout = 3.3V
Cin = 100uF, 25V, 20%,Tantalum and 22uF, 25V,20% Ceramic
Cout = 100uF, 6.3V, 20%, 70mOHM ESR, Tantalum and 100nF ceramic
Radj = 1.87K OHM
My queries :
1. Whether this design works for current requirement of 2A? The voltage deviation expected at the regulator output is 100mV
2. The Cout is 100uF, tantalum with ESR = 70mOHM. Whether this ESR is high for the requirement?
3. Can i go for 300uF ? If yes whether I can keep the ESR same or should I change? if chang, lesser or higher value?
Please suggest me these details.
Regards,
Vijetha