Other Parts Discussed in Thread: TPS92511, TPS92513
Hi,
I am using TPS92511 for a fast LED flashing application (20uS on , 2500uS off) and reading the response (reflection) with high accuracy.
Due to the sensitive nature of the measurement, minimizing the ripple during the on-time is very desirable.
Based on my knowledge of buck converters and according to datasheet, there are two option to decrease the ripple:
A- Increase the inductance value
B- Use an output capacitor (in parallel with LEDs)
Here are my questions:
1- Is there a limit (maximum value) for the inductor?
2- Is there a limit (maximum value) for the output capacitor?
3- How these parameters (inductance and output capacitance) affect the rise/fall time of the LED current?
Ideally I want the LED current to be as close to a square wave (20uS on - 250uS off) as possible, with minimal ripple.
Note1: I have used similar values in the datasheet (8.2: Typical application) with no output capacitor, so a large ripple (25%) is expected. For the next iteration, I am trying to minimize this ripple while not affecting the rise/fal times.
Note2: To further clarify, I am using the PWM dim input to switch the current on/off (I am applying 20uS ON time which is longer than the minimum pulse width of around 6uS). I use the Iadj pin for analog dimming (injecting current).
Note3: In reply to Niq question "TPS92513 ripple Current Requirements", Clinton responds: "you can use an output capacitor and the LED ripple current can be as small as you want to make it." 
Thanks